Other Parts Discussed in Thread: BQ76930, BQ78350, BQ76920
在用bq76930+bq78350进行锂电池保护时,可不可以在边充电边放电时,连接上位机bqstadio软件 进行检测?求教
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Michael,我在使用bq76920进行激活是,我短接了ts与v2,而datasheet上是短接ts与v1,这样对芯片有影响吗?
短接TS与V1时,中间要接一个10K欧姆的限流保护电阻。短接TS2与V2是否能退出Ship模式我没有实际验证过,你短路了以后是否退出ship模式了,如果没有成功就用在串联10欧姆电阻后,将TS1与V1连接。
感谢你的回复,Michael ,我的板子上并没有10k的限流电阻,短接v2后,板子可以通讯,应该是退出ship模式了吧,但是我短接v2后,下次再短接v1,为什么板子就不能通讯了?是不是因为我短接v2的原因?谢谢
TI的工程師:
你好,我在使用EV2300和BQ76930通訊的時候出現如下報錯
err:Unable for read iic ADC and offset from connected device.please ensure a powered bq76930 is conneced to the iic communications lines on the communication adapter and slave address is correct. restart this tool when resolved .you may continue but defualt values for ADC offset will be used.
這是是什麼問題?
此种情况我也遇到过,大部分是模拟前端BQ76930单节电压采集有问题。