您好,目前遇到的问题是使用BQ25672充电,NTC并非紧贴电池,密闭的空间很快会让充电电流下降至800mA左右(12V输入),默认设置是12V 1500mA充电。后面将NTC紧贴电池,充电温度阈值范围内,就是说电池温度并没有达到温度阈值。由于结构以及接口固定,能否通过寄存器提高高温阈值以改善充电问题。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
https://www.ti.com/lit/ds/symlink/bq25672.pdf
8.5.1.19 REG16_Temperature_Control Register (Offset = 16h) [reset = C0h]
请看这个部分有详细说明,请您参考。