1:如何修改充电温度阈值?
2:如何获取实时温度?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我通过  REG0x1B_NTC_Control_1 寄存器地址,获取得到 截图里的温度阈值 ,我的问题是,
,我的问题是,
TH4 is 35°C, TH5 is 45°C, TH6 is 60°C (default) ,这里的TH4 TH5 TH6 为什么会有3个温度值呢?分别代表什么意思呢?如果我要设置温度阈值是43°C该如何设置呢?
您好
数据手册里面Figure 8-3. TS Charging Values有写programmable

下方链接中包含有计算工具,您可以尝试修改。