This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC384X的斜率补偿时CT脚充电电压值是怎样算出来的



我想问一下用UC384X做开关电源时,电路的斜率补偿时有个参数不会算,请高手指教一下?就是上面附件中的最后一页的Vosc(晶振充电时的坡度)中的d(Vosc)=2,Ton=12.3这两个值是怎样得出的?

楼主,这里dVosc是CT上的充电电压,最终充到2V,CT充电的时间是近似是开关周期(减去死区时间),近似计算CT电压上升的斜率为2/(12.5-0.145)=0.17V/us

上面是我之前发的一个帖子问的问题还有附件,我现在还想问一下就是这个dVosc是怎样算出来的,是不是用的这个公式dvosc=Δv/Δt(Δt=0.45RtCt),如果是的话,我想问一下这个Δv值是怎样取的?

电流控制技术和斜坡补偿.pdf