This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: X038 battery pack chemistry ID issue

Part Number: BQ40Z50-R1

As requested, use 0.5c charge, 0.1c discharge, 4s capture data. After uploading to the website, the return message shows too large a difference between the data in the current chemical ID table, as shown in the attachment, suggesting that there is no suitable current no suitable chemical is for selection. What should I do about this? Do I need to change the charge/discharge conditions to redo the data?X0384214-report.zipX0384214.zip

x 出现错误。请重试或与管理员联系。