Other Parts Discussed in Thread: TPS61230, BQ25100
我想给一个采集板供电
输入:外部24V电源和2块锂电池(8.2V)
输出为:5V
电流1A
工作条件:不接外部电源的时候锂电池给板子供电,接入外部电源的时候既能给板子供电又能给电池充电
要求:芯片越小越好,外部电路越简单越好。(对尺寸比较敏感)
多谢多谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
楼主,你这种应用,最好的做法是使用一个简单的charger再带一个boost芯片。电池采用两节并联接法,不要串接。在24V不接的情况下,电池通过升压芯片升到5V,给后级系统供电,在24V进来的时候,通过charger 给电池充电,同时经过后边的升压芯片给系统供电。charger推荐使用BQ25100,升压芯片可以看一下TPS61230. 如果不这样,24V到8.2V需要个降压,8.2V到5V同样需要一个降压,而且24到8.2V的降压还不一定带有充电管理功能,充电效果也不会很好。