在使用ADS1256时,使用datasheet推荐的参考电压电路,如图一所示:
但是在实际使用时,发现R142上焊接一个1K的电阻时,Vref为2.0V;R142位置上焊接3K电阻时,Vref电压为2.1V。不得不,我只能焊接在R142的位置上,焊接一个0欧姆的电阻,Vref的电压才约为2.5V。这是为什么呢?(难道是ADS1256的datasheet上是错误的,还是这颗运放的原因?)望各位大神指点一下。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
现在把REF5025后面的运放OPA2376,电阻R142,电容全部去掉,REF5025的6脚输出还是一个频率为750KHz左右的正弦波(已更换过REF5025)