This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54620: 同步信号设计

Part Number: TPS54620


你好:

在使用TPS54620的CLK模式与RT模式切换时,在连接配置RT电阻之后,外部时钟是否可以直接连接RT/CLK这个引脚,还是要做AC耦合?

  • 感谢您对TI产品的关注!
    关于你的咨询,在使用TPS54620的CLK模式与RT模式切换时,外部时钟信号可以直接连接到RT/CLK引脚。

    但是如果通过AC耦合来连接会更好些。
    因为AC耦合可以防止直流偏置电压对时钟信号的影响,从而确保时钟信号的稳定性和准确性。

  • 谢谢回答,我们现在同步时钟是FPGA给出,而FPGA上电只有就能够按照逻辑输出同步时钟的,是拉高或拉低,以及可能出现的不规则的跳变。那么这个时候相当于同步时钟输入相当于接地、上拉,这个时候,TPS54620可以按照RT(外置电阻)的方式运行吗?DCDC的输出会出现异常吗?

  • 谢谢回答,我们现在同步时钟是FPGA给出,而FPGA上电不是马上按照逻辑输出同步时钟的,而是拉高或拉低,或者可能出现的不规则的跳变。那么这个时候相当于同步时钟输入相当于接地、上拉,这个时候,TPS54620可以按照RT(外置电阻)的方式运行吗?DCDC的输出会出现异常吗?

  • 单凭描述无法给出判断,最好实际测一下。