This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3820-Q1: 器件WDI引脚使用问题咨询?

Part Number: TPS3820-Q1
Other Parts Discussed in Thread: TPS3820

此芯片在说明里面有描述这段文字;

The watchdog timer can be disabled by disconnecting the WDI pin from the system. If the WDI pin detects that it is in a high-impedance state the TPS3820/3/4/8-xx-Q1 will generate its own WDI pulse to ensure that RESET

does not assert. If this behavior is not desired place a 1-kΩ resistor from WDI to ground. This resistor will help ensure that the TPS3820/3/4/8-xx-Q1 detects that WDI is not in a high-impedance state.

这里描述,如果芯片WDI引脚检测到高阻抗,则内部产生时钟,防止发生复位事件。

请问,这个逻辑或者功能,主要是考虑到什么因素,有这个功能。