This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61070输出电压问题

大神好! 请教一下:使用TPS61070设计一款升压器,输入两节电池供电,2.0V---3.0V,要求输出5.0V

使用电感:VLS4012  4.7uH/890mA; 分压电阻:274k/30.1k;输入出电容:10uF;

出现了输出电压5V到5.5V变化,空载时频率低一些,输出25mA时见下图。

用示波器测量pin1(SW)端时,改变了电路参数,输出波形变化为下图

 

把电感改为10uH后,输出正常。为什么电感4.7uH不行?增大电感,会减弱输出能力。