你好,使用该器件进行DCDC电路时,在Vin=12V的情况下,允许的输出的最大电压和电流是多少?是否有对应的计算公式?
另:下图1-2为TPS54560DDAR手册中关于Vout宇Vin和Iout的计算公式,图3为当前设计原理图(Vout=11V,Iout=3.6A,Vin=12V)



This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
使用该器件进行DCDC电路时,在Vin=12V的情况下,允许的输出的最大电压和电流是多少?是否有对应的计算公式?


详细资料请您参考datasheet有更详细的公式和说明

您也可以在官方这个IC主页下使用如上图工具帮您辅助设计。以下是官方这个IC的链接。