This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28070: UCC28070交错PFC,高压230VAC输入时,电感上电流峰值出现削顶现象

Part Number: UCC28070

采用UCC28070设计1800W电源,现在230VAC输入,带到1200W时,测试单路电感电流,感觉整个电流包络的峰值被限制了一样,然后整个输入电流的波形下半部分不是很光滑,但是电源PF值正常,为0.994,请问这个电流波形正常吗?

备注:黄色的是总的电流波形,可以看到黄色波形的下半部分电流波形不规则, 绿色的是单路PFC电感上的电流波形,可以看到顶部视乎被限制了