我现在的需求是:27V输入 输出 32V@0.5A 50V@1.8A 100V@0.01A
目前选型是使用LM3478,我通过WEBENCH模拟了一下,有如下几个问题:
1.模拟的时候只要输出50V时,都无法模拟,改小电流也不行。
2.输出100V时,显示转化效率不足70%,有什么优化方案么。
3.输出功率比较大时需要注意哪些因素,有没有相关的手册资料推介。
另外对于我上面的需求,有求他的推介芯片或者方案么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
2.输出100V时,显示转化效率不足70%,有什么优化方案么?
你好,因为你的电压比较高且输出电流很小,因此开关损耗占主要部分,需要轻载降频芯片,但是这颗芯片没有这个功能,有这个功能的芯片,耐压不够,且成本较高,如LM5122。
3.你好,输出功率比较大时,注意寄生电感和结电容震荡造成SW脚电压尖峰。布线时需要注意一下,具体参考LM3478芯片资料的layout example即可,谢谢。