Other Parts Discussed in Thread: TPS74701
请问下TI LDO的BIAS引脚是一个什么功能,与EN使能引脚差不多?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
楼主,LDO的BIAS引脚用于给内部的运放,逻辑电路,FET的驱动级供电。如果有低dropout的需求,可以额外给BIAS供电,让VBIAS>VOUT+一个固定的电压(规格书中有标明),可以让输入和输出的压差更低。以TPS74701为例,在VBIAS>VOUT+1.62V时,dropout的电压可以低至50mV,而如果VBIAS和VIN连接在一起,那么dropout需要达到1.31V。
你好,主要是为了兼顾损耗和性能指标(如PSRR,transient)。高电压BIAS来给控制和高性能电路供电,Vin来给输出功率,谢谢。