This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7480-Q1: EN/UVLO control issue

Part Number: LM7480-Q1
Other Parts Discussed in Thread: LM7480

Hi TI TEAM

根据规格书描述要进入低功耗模式,需要将EN/UVLO引脚拉低,可以通过MCU IO去控制。然而,EN/UVLO的最小值是0.3V,而大多数MCU规格的VOL,也就是输出低电平给的规格最大值是0.4V,也就是说在最差情况下,MCU控制EN/UVLO引脚,有可能不能将LM7480驱动到足够的低电平,从而无法进入low iq模式。这个问题TI这边如何理解,内部看结构应该是个比较器,为什么EN/UVLO的范围那么大,0.3~0.93V区间?