This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5176: 使用过程中,当输入电压大于27V时,芯片容易出现损坏的情况

Part Number: LM5176

使用LM5176作为INTEL 12代ALDER LAKE主板的主输入电源时,电压输入范围是9V~36V,输出电压为12V.。 当输入电压大于27V时,在开机时CPU上电瞬间容易出现芯片损坏的情况; 用万用表测量损坏后的芯片引脚阻抗,LDRV1引脚的阻抗的电平变低出现异常。 

用示波器测量LDRV1引脚,和HDRV1引脚波形,当输入电压超过27V时在CPU上电瞬间,这两个引脚的波形出现很不稳定的杂波,随着输入电压的升高,这个杂波也越来越大,到一定程度或多次上电,芯片就损坏。

如附件所示为上电时HDRV1引脚的波形。

  • 感谢您对TI产品的关注!
    关于你的咨询,有可能纹波造成芯片损坏了。
    你看看webench tool生成的设计,跟你的设计比较一下,排查下问题点。
    webench生成的电路点击无源器件,有推荐型号。
    你重点看看电感,MOS等的推荐型号和参数。

    webench.ti.com/.../285