When using the backup drive channel to detect temperature with NTC, ENOUTXn is 1 and PWM is maximum. Will the chip report an open circuit fault?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When using the backup drive channel to detect temperature with NTC, ENOUTXn is 1 and PWM is maximum. Will the chip report an open circuit fault?
Hi,
What is your channel voltage range? PWM is maximum means 100%?
Please see the LED open-circuit fault detection criteria, and 6.3.6.8 LED Open-Circuit Diagnostics in NORMAL state of the datasheet. The open fault can be triggered under certain conditions. Many thanks!