This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
要求输入9-24V输入,12V、5V 1.5A输出,要有输出端短路保护功能。
亲;需要隔离的还是非隔离方案。
这个不是很懂啊,隔离非隔离有什么区别啊。刚刚接触这块,请赐教!!
亲;隔离呐;就是输入和输出是绝缘的。非隔离的不是,入出共地。
因为12V输出对于输入电压范围属于buck-boost,暂时没有buck和buck-boost集成在一起的方案
如果是隔离方案,推荐LM5022
感觉这个LM5022刚刚通电的时候输出电压会不会很大啊。我要做的话,前后级可以共地的,不用隔离也可以。TI有没有双输出的芯片啊,同时输出+5V和+12V的啊。
用两个LM2596怎么样啊!!但是好像没有短路保护哦!