Other Parts Discussed in Thread: BQ24600
大家好,
我使用BQ24600做聚合物锂电池充电器,电池是4串,4.2V*4,输入是24V左右,BQ24600驱动两颗SIR426DP,充电电流2A。
PCB使用4层,中间两层是完整地,BQ24600热焊盘焊接且通过5个0.4mm过孔连接到PCB的中间地线层上
现不充电时(EN=0),BQ24600及MOSFET无温度。EN=1时,充电功能正常,观察波形除了MOSFET振铃过冲稍大,各点波形均正常。
但是电路温度迅速升高,普通室温,自然风冷时使用红外测温,芯片和MOSFET区域温度为65摄氏度,实际芯片温度应该更加高一些,感觉温度高,麻烦评估下这个温升正常吗?