您好,调试过程遇到了几个问题:
- 请问该器件的开发板TPS23754EVM-383推荐了一款信号为PA2649NL的变压器,是否可以用于基于 TPS23754EVM-420EVM设计的12V输出的反激降压转换器的设计中;
- 调试过程中发现VCS可能会达到5V,但手册给出该引脚阈值是550mV左右,达到阈值后应该会关断MOS,但MOS管没有动作,这个可能的原因是什么呢,芯片损坏了吗
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
请问该器件的开发板TPS23754EVM-383推荐了一款信号为PA2649NL的变压器,是否可以用于基于 TPS23754EVM-420EVM设计的12V输出的反激降压转换器的设计中;
不建议,因为在TPS23754EVM-420EVM有推荐的变压器型号POE300F-50L,且它俩的电气参数上有区别。
调试过程中发现VCS可能会达到5V,但手册给出该引脚阈值是550mV左右,达到阈值后应该会关断MOS,但MOS管没有动作,这个可能的原因是什么呢,芯片损坏了吗

您看一下这个表VCS是可以达到5V,因为它的参考是与[ARTN, COM的压差最大可以达到Vb,而您指出的是官方在测试条件下相对于GND的参考值,所以如果您单论它能不能达到5V需要看参考。
谢谢,目前使用PA2649NL能够输出12V了,之前可能是某处焊接存在问题。但现在还存在有一些问题:
1、POE300F-50L是5V输出的变压器,如果需要输出12V是需要替换成POE300F-12L吧,出变压器外这里仅需要修改反馈电路部分,而其他部分不用做修改吧。
2、如果想继续使用PA2649NL这款变压器的话,需要进行那些测试来保证这款变压器在这个设计中能够长时间稳定运行呢。
3、测试采样电阻的电压电压波形比较奇怪,在栅极关断过程中采样电阻电压有一个明显的回弹电压,采用了二极管加快关断过程也没有明显的改善,不确定是不是由于晶体管寄生电容过大导致的,请问有没有什么改进建议,目前是想尽可能在后续找不到合适晶体管时也能消除这部分的影响。另外这里的波形是否表现为变压器饱和呢,感觉和常见的波形有一些区别。蓝色是栅极驱动波形,黄色是电流传感电阻的波形
您好
1、POE300F-50L是5V输出的变压器,如果需要输出12V是需要替换成POE300F-12L吧,出变压器外这里仅需要修改反馈电路部分,而其他部分不用做修改吧。
建议进行相应的匹配修改。因为之前的是5V ,您现在要换成12V,变压周围以及输出都要做匹配修改。
2、如果想继续使用PA2649NL这款变压器的话,需要进行那些测试来保证这款变压器在这个设计中能够长时间稳定运行呢。
一般会做极限测试和长期运行测试,在电路上做相关的保护电路。
3、测试采样电阻的电压电压波形比较奇怪,在栅极关断过程中采样电阻电压有一个明显的回弹电压,采用了二极管加快关断过程也没有明显的改善,不确定是不是由于晶体管寄生电容过大导致的,请问有没有什么改进建议,目前是想尽可能在后续找不到合适晶体管时也能消除这部分的影响。另外这里的波形是否表现为变压器饱和呢,感觉和常见的波形有一些区别。蓝色是栅极驱动波形,黄色是电流传感电阻的波形
TPS23754测试问题分析及改进建议
采样电阻电压波形异常