This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于使用TI公司CSD18531和18533芯片实现四管Buck-Boost变换器高效率同步整流问题

Other Parts Discussed in Thread: LM5175

尊敬的TI技术人员你们好,

  最近在研究四管Buck-Boost变换器。根据你们LM5175 EVM User‘s Guide中提供的硬件设计资料,我选择使用CSD18531,CSD18533作为mos管。但是为了实现灵活的控制,我使用IR2110作为驱动芯片,28335作为数字控制核心,在开环状态下发出我想要的占空比信号。

原理图设计:

PCB设计:

我目前采用的策略是Q1和Q2采用一组同样信号控制,Q3和Q4采用另一组互补信号控制,实现电感的储能和放能。工作频率为50kHz。

实际中,Q1管的损耗非常大,具有很明显的开关震荡,因此我认为是因为开关震荡造成了开关损耗。

产生这样的原因可能与驱动有关,因为驱动经过300ns才从0V上升至15V。另外也可能与电路的某些参数有关。实际中,我驱动使用的二极管为5819。

我非常迫切的希望得到您们的帮助和建议。当前情况下电路效率仅81%,远没达到LM5175所能达到的95%以上的效率,因此我的设计必然存在问题。

劳驾各位不吝赐教~