This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我使用12V5A供电,使用TPS43060升压至26V,再使用LM5148降压,实现12V转5~24V可调输出,原理图如下
TPS43060和LM5148输出电压均正常,开关频率TPS43060-500kHz, LM5148-500kHz
空载时TPS43060温度在45℃,LM5148温度30℃;
输出12V,施加45W负载时,TPS43060和上下mos管(M1, M2)温度最高90℃,LM5148和上下mos管(M3, M4)温度最高60℃。
请问TPS43060的异常发热该怎么解决
您好,根据您的描述,建议选用较小Rds on 的mos, 同时做好散热。希望对您有帮助.
另外您可以使用webech工具,验证您的设计和选用对应的器件。
webench.ti.com/.../297