This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76972: The RST_SHUT pin was used to reset, but the previously set parameters did not fully restore the default values

Part Number: BQ76972


hi:

use chip: BQ7697204

Configure the chip to enable REG1 to output 5V, REG2 to output 1.8V, and then reset via the RST_SHUT pin: Pull the RST_SHUT pin up 300ms and pull it down again, and find that the REG1 output can only recover from 5V to the default 3.3V, but REG2 still outputs 1.8V.

Shouldn't REG2 revert to the default output 0V after reset?

Is this a normal phenomenon? Is it because the reset does not change the output parameters of RGE2?