Part Number: TL431C
Other Parts Discussed in Thread: TL431
我想做一个TL431+PC817的LLC的光耦隔离反馈环。进行原理性认证时将VO设置为5V,Vd供电电压为3V,经过计算(U0-1)/R3=If,我将If最大值设置为了8.5mA。PC817C的放大倍数在100%到400%,最大值为50mA,但经过测试,我调整VO输出的电压,正常来说COM端电压会因为电流的改变带来改变,但是COM端无电压,最大也就是10mV,继续测试TL431后发现Vref与地间的电压是-2.47V,而不是正的2.5V,想请问这是什么问题。或者有什么建议吗。谢谢。