Other Parts Discussed in Thread: BQ24192, BQ25895, BQ24133
最近在设计一款充电电路 电池容量10Ah左右 所以需要大电流充电 看了BQ24192 BQ24292好像都是支持USB与电源适配器的 但是不明白电流是怎么设置的 我打算USB输入时输入5V 1A 而输入电源适配器时输入12V 1A 这样通过片内DC-DC电路之后就可以得到更大的充电电流 看了数据表好像是只能直接设置输出电流的 请问各位可以设置输入电流吗?先谢谢各位了。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好。在回答你的问题前,先跟你确认下:BQ24192中文手册里的USB输入是指电脑的USB口,适配器是指手机充电器之类。你说的USB输入5V/1A是指哪一个?1A不是电脑USB口的标准。12V/1A是适配器固定电压吗?还是QC2.0的高压快充适配器产生的5V/9V/12V?USB、适配器是同一路还是分开两路?通过什么来识别?
如果是同一路的、你想要的高压大功率输入是基于快充适配器的,那建议你用BQ25895,能够通过自带D+D-握手把适配器电压升到12V。
如果是分开两路输入源、通过或逻辑输入给BQ24192的,那要设置不同输入源对应不同输入电流的话,则需要MCU识别不同的输入源,然后写BQ24192的寄存器I2C REG00[2:0]。
如果想比较简单的充电,可以使用一些不需要I2C控制的充电芯片,像BQ24133一类。