This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5148: 12V转5V降压模块,输出空载时正常,连接负载后会掉电保护的问题

Part Number: LM5148


使用webench生成的降压电路,设计需求是12V转5V10A;

目前上电不接负载时输出电压正常,此时只有一颗LED而已,大概20mA左右,接入负载后自动掉电,哪怕只连接1W的小负载也不行;

检测时发现芯片Vcc始终是5V,en脚电压2V,连接负载时上端功率mos栅极控制信号被拉低,输出断开;

这种现象符合规格书中描述的ISNS+端到Vout的峰值电压超过60mV时,立即停止HO输出,即关断上功率mos,但是我当时测试的输出电流只有200mA不到。

输出端的电流检测电阻使用的是两个2512/10mΩ电阻并联,理论上电流应该能达到10A,现在没办法确认问题出在哪里

以下为原理图和Layout图:

以下是webench生成的参考原理图