Other Parts Discussed in Thread: TPS65261-1
您好:
我这边用TPS65261-1这款DCDC芯片设计一个8V到3.3V的降压转换器,输出电流要求是1.5A,我们按照DataSheet上给的原理图设计的PCB,由于PCB设计问题(PCB上封装画的偏大),导致芯片是通过一个两层的小转接板转到PCB上的。现在测试发现它只能提供约500mA的电流,超过500mA的情况下输出电压就会降到很低,芯片自动进入断电保护状态。现在怀疑两个地方可能有问题,一是转接板会不会不能走大电流,还有就是上面一个4.7uH的电感,我们采样的是Murata的一款叫做:LQM2HPN4R7MG0的型号电感。我想问一下我们现在看到的这个现象可能是什么原因导致的?谢谢!