This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23523: How to apply it to combine two -15V sources into one?”

Part Number: TPS23523
Other Parts Discussed in Thread: UCC29002

“How can the TPS23523 be used to first hot-swap two -15V power supplies and then OR them to the load?

Currently, I need to combine the -15V outputs from two PSUs into a single output, so that when one PSU fails, the other PSU’s -15V can immediately supply power to the load.

If there are other ICs that are better suited to my application, please let me know and explain how to use them.

Thank you!”