BQ76920欠压保护设置为2.7V,但是去测量发现欠压保护大概为2.95V,有什么原因吗谢谢

TRANSLATE with x
English
TRANSLATE with
Enable collaborative features and customize widget: Bing Webmaster Portal
Back
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ76920欠压保护设置为2.7V,但是去测量发现欠压保护大概为2.95V,有什么原因吗谢谢

您好
关于你提到的BQ76920欠压保护设置不准确的问题,即设置为2.7V但实际测量发现欠压保护大概在2.95V,这里有几个可能的原因和排查方向:
VC引脚连接不正确:BQ76920的VC引脚用于连接电池单元,以确保正确监测电池电压。如果你的BQ76920是用于4串电池组,那么VC3-VC4应该短接,而VC4-VC5不应该短接。如果VC引脚连接不正确,即使电压读数准确,也可能会触发UV(欠压)警报。因此,请检查你的VC引脚连接是否符合数据表中的要求。
电池连接问题:除了VC引脚外,还需要检查电池的连接是否牢固、正确。如果电池连接不良或存在断路、短路等问题,也可能导致欠压保护不准确。
软件配置错误:BQ76920的欠压保护设置通常是通过软件配置的。如果你的软件配置不正确,比如设置的欠压阈值与实际不符,或者相关参数没有正确配置,也可能导致欠压保护不准确。因此,请检查你的软件配置是否正确。
针对以上可能的原因,我建议你按照以下步骤进行排查:
您好
BQ76920欠压保护实际值高于设定值(2.7V)而为2.95V,可能的原因包括:电池状态影响、测量误差、设备校准问题以及保护机制设定。