This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76972: For not using cell pin, and the pins are short, set the Settings: Configuration: what are the benefits of Vcell Mode?

Part Number: BQ76972

hello:

I do not use the chip's 6, 7, 8, 9, 10 cell voltage acquisition channels and short-connect them. I whether it is necessary to set the Settings: Configuration: Vcell Mode register, can make use of the protection of the feet. What are the advantages of setting this register, which will be more conducive to the sampling accuracy of other circuits? Or prevent external abnormal inputs from entering the chip through unused cell voltage acquisition pins and cause chip damage?

x 出现错误。请重试或与管理员联系。