This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Attached is the FW PJT file for our model X580WNx. After exporting the VIF file using the latest version "TPS65993_4 Application Customization 6.4.35", the differences compared to the version required by the testing vendor are significant. After a round of testing,"http://share.graniteriverlabs.com.tw/sharing/sBtqppo8k" many items still cannot meet the current requirements of the VIF version 3.1.1.7, and these items cannot be easily modified through the VIF Editor, as they need to correspond to the PJT and BIN files.
0333.x580_TBT5_F909p12p15_30DA_20240902.pjt
I have inquired with the team that handled the previous X370 model, who encountered the same issue as us. At that time, TI provided the new versions of the VIF, PJT, and BIN files, which were then given to the testing vendor for validation.
Could you please assist in providing the latest VIF 3.1.1.7-related files?