Part Number: TPS2491
TPS2491的工作中,ILIM的设定具有优先级,会覆盖功率限制计算出的最大电流值。如果ILIM设置的值低于功率限制计算出的电流,TPS2491会以ILIM的值作为最大电流限制,确保输出电流不会超过ILIM设定的上限。是这样吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS2491
TPS2491的工作中,ILIM的设定具有优先级,会覆盖功率限制计算出的最大电流值。如果ILIM设置的值低于功率限制计算出的电流,TPS2491会以ILIM的值作为最大电流限制,确保输出电流不会超过ILIM设定的上限。是这样吗?
您好,
是的,一般使用使用VCL为25mv进行计算

正如你说,我一直疑惑手册的这一条怎么理解,是这样理解吗:功率限制的时候最大电流为25mV/R,正常限流是50mv/R,也就是功率限制的时候其最大电流是ILIM的一半对吗?所以更不存在功率限制时电流超过ILIM啦,对吗?
功率限制状态:当设备处于功率限制状态时,电流限制的典型阈值为25mV/R
正常限流状态:在正常限流状态下,电流限制典型的阈值为50mV/R
详细请查看下面的链接