This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我使用LM5123设计一款产品,需要用到12V升压到24V为TAS6424E供电,但是我发现升压后影响其他12V供电的功放芯片正常输出,在输出过程中经常被其他信号所打断,而产生震荡。
这是原理图和PCB布局,不知道哪里有问题。
下图是正常输出正弦波时被打断的信号
更奇怪的是,另外一颗距离升压电路较远的12V供电输出的功放芯片没问题,但是离的近的这颗总是被干扰。我怀疑是没有把AGND和GND单点接地的原因,但是不应该产生这么大的干扰吧?
您好,根据您的描述,给您几点layout建议:1.开关大电流环路尽量短。2 信号地和大电流地单独走线,并在芯片GND引脚单点连接。3.输入高频电容器要里离芯片输入引脚尽可能近。 4.电感推荐使用屏蔽电感器。
布局和芯片选择可以参考TI提供的开发板。
还有个建议,多焊接一块板子进行评估,避免因为个别器件品质问题影响排查问题。从您的描述看是一个EMI问题,只能从layout入手逐条逐线排查。希望对您有帮助。