This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq76PL455A-Q1 评估模块 GUI功能性测试



    bq76PL455A-Q1 评估模块 GUI的TTL-RS232的串口测试问题,SW2拨到SINGLE, SW1的1为ON,其余2、3、4为OUT, J3的6根引脚与USB-TTL转换器连接,其中J3的 1脚外接的串口GND,3脚外接5.0V, 4脚外接RX,5脚外接TX,2、6脚未接,J1端子分别接的16串3.0V的单体电池,bq76PL455_GUI软件安装成功,TTL-RS232驱动已经安装成功,电脑也能识别到COM口,但是模块上电后不能打开串口,显示“unable to open com port”,请问J3的2、6脚是否要连接,或其它地方需要设置?谢谢!