This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23881: 如何将2线对端口最大功率设置为45W

Part Number: TPS23881


如题所述,电路实际设计为2线对端口,目前软件设计为auto模式,

查看手册描述(图1)2线对Pcut可编程功率为2W ~ 65W,但是在0x29寄存器中配置端口最大功率时,2线对最大也只能配置为30W,请问这个怎么理解呢,Pcut编程功率代表的意义是什么,如果这里能到65W,为什么端口最大功率配置2线对又只能到30W?

如果说2线对端口可以配置最大功率输出大于30W,比如设置为最大输出45W,应该怎么配置?是只需要寄存器配置还是需要修改硬件电路?

  • 设置Icut时,您可能需要进入手动模式。 或者,如果处于自动模式,则需要在端口打开后重写Icut。 Icut配置为2Ah和2Bh寄存器。 您需要Icut = 920 mA,在这种情况下,使用50 - 57V PSE输出电压,您可以将46W - 52.44W的功率保护阈值设置为超出。