Part Number: LM27402
Other Parts Discussed in Thread: LMV321, LM27403, TPS54331, LM5190
使用LMV321搭建恒流电路,设计指标为2毫欧电阻,20A电流,产生0.04V压降,20A量程下LMV321反馈给LM27402芯片FB引脚为0.6V
27402 VDD引脚4.5V为LMV321供电,目前输出无法达到恒流状态(输出电流一旦达到20A,运放输出电压超过0.6V无法稳定输出给FB,导致恒流失败),特意上论坛求问,谢谢!
下面附上原理图和计算步骤




目前按照设计重新设计了CC/CV环路,请给出建议!谢谢
,已经制作成功了,可惜LMV321 失调电压过大,造成放大误差挺大的,另外我需要求解如果使用专用电流放大器,该怎么配置增益?以INA181A2为例,50vv的增益,在不更换检流电阻的情况下, 20A的放大电压会达到5V,是否可采用分压电阻来调整电压?要不提供一下最佳解决思路,thanks!