This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01606: 關於輸入的頻率問題?

Part Number: TIDA-01606

Hi, 非常感謝您的幫忙。

關於TINV_UNIVERSAL_GRID_MAX_FREQ的最大上限這個值可以設到多少 ?

之前沒有說明清楚,我們並不是要輸出超過60Hz的頻率,因為這是雙向的系統,

我們有一台發電機的輸出是100 ~380Hz的3向交流電,所以我們透過tida-01606來將這個輸入的電源轉化成DC電源。

所以想要知道當做為輸入時, TINV_UNIVERSAL_GRID_MAX_FREQ的最大頻率可以到多少?

麻煩您了,感謝!