Other Parts Discussed in Thread: LP5891
我在LP5891-Q1的规格书中有看到建立一个LED(240*180)显示模块的例子,上面有说需要用到96个LP5891,并且需要8个级联(类似于一行有16个LP5891)。
我想问的具体如下:
1. 上面这96个驱动只用一个SCLK,一个SIN,一个SOUT线就可以控制所有的驱动吗,也就是说MCU端只需要一路SPI通讯?还是说每多少个驱动(例如,32个)就需要一个SCLK,一个SIN和一个SOUT线,需要MCU端支持很多路的SPI通讯?
2. 上面的这个“8个级联”有数量限制吗?(例如,最多只能是16,不能超过16之类的)
3. 这个LED显示模块的例子是每两个LP5891为一组,那么是否可以每4个为一组呢?
4. 规格书中有“This protocol can support up to 32 devices cascaded in a data chain”,这句话如何理解?是一行最多不能超过32个LP5891?还是说每32个LP5891就需要有一路SPI通讯去控制这32个驱动?