This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65910a1的VAUX2的 输出电流有多大?



TPS65910a1的VAUX2的 输出电流有多大?   最开始的手册 标明为 150mA,  但最新的SWCS046S里提到将此LDO 从150mA变更为300mA

问题一:但是我看见有的参考设计 ,VAUX2为所有3v3供电, 例如:ICE的原理图。    但发现现在网站上的原理图都是 3V3单独使用LDO产生的。这是为什么?

问题二:现在我的设计AM3352ZCZD60和TPS65910A1, 65910的文档里提到“SEL = 10, IOUT = 0 to 100 mA”  ,那就不是150或300了啊???

问题三:我现在设计VAUX2为单板的所有3V3芯片供电,3V3上的有3352的VDDSHV6+2片 KSZ8041(变压器中心抽头,单独LDO供电)+nand flash+SPI FLASH+12颗指示灯。  在生产时候,现碰见多片板子,有短路现象,但不是VAUX2, 短路的如 VDAC或VPLL等等,这是为什么呢?