This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教BQ500212A的使用问题



完全照搬TIDA-00334的原理图,因产品尺寸问题,PCB图重新布局。

单独测试该线路板未测试到500ms的握手信号,反而有50Hz。

请问这一般是哪里的问题?还有snooze和sleep的RC时间常数怎么计算?跟哪个电阻电容有关?

Schematic.pdf
  • 经测试,应该是3.3V每隔20ms被拉低一次,2V左右,导致芯片不能正常工作。

    将3.3V用外部稳压电源供电,芯片3.3V正常,此时在线圈上可监测到500ms的握手信号。

    请问一般什么情况会导致3.3V被拉低呢?我没用文档推荐的LDO,用的是TPS78233,会有问题吗?

    怀疑瞬间启动电流大,改用输出电流3A的LT1085也不行。

  • PWM_A,PWM_B什么都不接的情况下,输出波形应该是正确的,间隔500ms;

    接上后续电路后,输出波形就变为间隔20ms了。

    求解。