Other Parts Discussed in Thread: UCC28070


下午好!想了解一下,用两块UCC5350MC-Q1配合UCC28070驱动
SiC MOSFET的话,1、如上2中接法都可以吗?哪种更好?2、上图中的RZ和稳压管的值怎么选择?如果希望
SiC MOSFET的截至电压为-5.1V,那么这稳压管的值选为5.1V吗?此时这芯片的GND悬空?3、我现在非隔离应用,用下图的话,那么GND1和VEE2可以直接连一起?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.


下午好!想了解一下,用两块UCC5350MC-Q1配合UCC28070驱动
SiC MOSFET的话,1、如上2中接法都可以吗?哪种更好?2、上图中的RZ和稳压管的值怎么选择?如果希望
SiC MOSFET的截至电压为-5.1V,那么这稳压管的值选为5.1V吗?此时这芯片的GND悬空?3、我现在非隔离应用,用下图的话,那么GND1和VEE2可以直接连一起?
您好
为了使齐纳二极管电路提供正确的负轨进行关断,输入需要是一个浮动的隔离电源,例如一个小型推挽式变压器(见下图)。齐纳二极管的阴极应连接到与IGBT发射极相同的节点,如图所示。
如果电路中的其他地方使用了接地,则不能如屏幕截图所示将VEE连接到地。除非您希望GND1和VEE2连接在一起,否则请关闭0V电源。
电阻器需要足够低,以允许齐纳二极管偏置到正确的电压。它不应该太低,以至于在稳定状态下耗尽你的孤立供应。
1mA通常是一个很好的电流目标。