您好,请帮我推荐一款(两款更好^_^),DCDC方案或芯片,非常感谢!
需求:
1、输入12~20V,额定输入15V,25A
2、输出55V,电流6A或以上
3、要求,效率高
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,多谢提示,我用webench设计了,我看了一些以往先关帖子,现遇到两个问题再请教一下(输入15V 输出55V6A)
1. 推荐芯片方案LM5123Q,当输出电822流大参数大时,比如6或7A,推荐的方案中mosfet的电压要求(154V)特别高,电流小(比如4A)电压要求就第80V,80V就比较好选mosfet,因为mosfet参数和价格选择也相对复杂,想问一下,要求Vds 154V的mosfet,我可以用80V的吗?或者说我选用输出参数4A,生成器件清单可以用80V的,实际使用超过6A会怎么样,该方案用于发电升压应用,可靠性要求还是比较高的场合。
2.LM5122也是可选方案,在效率上是否比LM5123Q低一些,或者技术老一点。LM5123Q最大输出是57V,我输出55V是否可以用LM5123Q,2V的冗余l量合适不。我想用更新的LM5123Q,是否推荐用LM5122呢?
3.用LM5123的话,麻烦请帮我看看这几个主要参数是正常的吗?电容数量多,电感值小和mos电压高等,不熟悉大功率电源,再次感谢老师!