LM5148的电源输入为27V/4A规格电源适配器,其输出设置为12V,在负载较轻时(大概200~300mA输出)表现一切正常,当带上1A以上负载时,芯片立刻无法输出且去除负载后VDDA、VCC均无法再正常输出电压,异常现象重新上下电无法恢复。麻烦帮忙看下,感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LM5148的电源输入为27V/4A规格电源适配器,其输出设置为12V,在负载较轻时(大概200~300mA输出)表现一切正常,当带上1A以上负载时,芯片立刻无法输出且去除负载后VDDA、VCC均无法再正常输出电压,异常现象重新上下电无法恢复。麻烦帮忙看下,感谢!
您好
LM5148是一款适用于高电流单输出应用的80V超低IQ同步降压直流/直流控制器。针对你遇到的问题,这里有几个可能的解决方案和建议:
检查电源设计:请确保你的电源设计符合LM5148的推荐设计,包括输入电压范围、输出电压设置、电感选择等。不合适的电源设计可能会导致芯片在重载时无法正常工作。
负载能力:LM5148支持大电流应用,但请确保你的负载在芯片的负载能力范围内。如果负载过大,可能会超出芯片的承受能力,导致芯片无法正常工作。
散热问题:在重载情况下,LM5148可能会产生较多的热量。请确保你的散热设计足够,以防止芯片过热导致损坏或性能下降。
芯片损坏:如果以上都没有问题,那么可能是芯片本身出现了损坏。请检查芯片是否有明显的物理损坏或过热痕迹。