故障一直显示,点击消除故障也没用,电池电压和温度也一直显示0.。。。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.请问你是连接BQ76930 EVM板还是自己的板?
2.I2C 上拉电阻是否添加?
3.所用的IC后缀是什么?BQ7693000/1/2/3的地址是0x08,BQ7693006的是0X18。
4.如果用的是EVM板,请按照BQ76930 EVM user's guide,2.2.1 AFE Quick Start步骤,去掉跳线帽,一步一步连接,是否成功通讯?
用的自己的板子,I2C的上拉电阻添加了的,通信地址是08,是可以通信的的,不然也不会检测到芯片故障的报警。。。。就是现在一直都是芯片故障,电压和温度都无法检测。。。
检测一下, CAp1到地 和 CAP2到-VC5X两端的电压, 是否都是3.3V。
如果有一个没有 , 就是芯片内部供电有问题。 TS1 he TS2 接两个10K电阻模拟NTC,
CAP1 和 CAP2 容值一定要一样。
1~5 , 6~10接电池接法要按照datasheet规定的。