This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76920: 关于BQ7692006PWR的唤醒方案

Part Number: BQ76920


BQ7692006PWR进入睡眠后,想插入充电器就唤醒,有什么设计方案可以参考吗,谢谢

  • 您好

    SHIP mode is the basic and lowest power mode that BQ769x0 supports. SHIP mode is automatically entered during initial pack assembly and after every POR event. When the device is in NORMAL mode, it may enter SHIP by the host controller through a specific sequence of I2C commands. In SHIP mode, only a minimum of blocks is turned on, including the VSTUP power supply and primal boot detector. Waking from SHIP mode to NORMAL mode requires pulling the TS1 pin greater than VBOOT, which triggers the device boot-up sequence. To enter SHIP mode from NORMAL mode, the [SHUT_A] and [SHUT_B] bits in the SYS_CTRL1 register must be written with specific patterns across two consecutive writes: • Write #1: [SHUT_A] = 0, [SHUT_B] = 1 • Write #2: [SHUT_A] = 1, [SHUT_B] = 0 Note that [SHUT_A] and [SHUT_B] should each be in a 0 state prior to executing the shutdown command above. If this specific sequence is entered into the device, the device transitions into SHIP mode. If any other sequence is written to the [SHUT_A] and [SHUT_B] bits or if either of the two patterns is not correctly entered, the device will not enter SHIP mode

    请您参考这个datasheet 中的说明来设计您所谓的唤醒过程。

  • 从SHIP模式唤醒到NORMAL模式需要拉动TS1引脚大于VBOOT,有什么文档可以参考

  • 您好

    关于这个IC的参考设计,官方只有开发板,以下是相关链接。

    www.ti.com.cn/.../BQ76920EVM