This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24650: 无法开始充电。

Part Number: BQ24650


使用BQ24650设计电路给电池组充电,输入电压27.3V,充电电压25V,充电电流800mA。电路原理图和PCB如下图所示。

现在出现问题描述如下:

1、电路无法给电池进行充电。径测试发现,控制MOS开断的PWM波形异常,每隔550ms出现无PWM驱动状态,持续时间约5ms。波形如下图所示,蓝色(通道2)为输出电压波形,黄色(通道1)为PH波形。

2、基于以上原因,导致输出波形如下图所示。