Other Parts Discussed in Thread: BQ24195
ti专员你们好: bq24195 sys引脚有什么作用,可以用做对外输出吗? 另外,在充电情况下,PMID输出电流可以达到多少? 在线等待,谢谢!This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: BQ24195
ti专员你们好: bq24195 sys引脚有什么作用,可以用做对外输出吗? 另外,在充电情况下,PMID输出电流可以达到多少? 在线等待,谢谢!SYS引脚可以用来给系统供电,比如MCU,电压范围一般在3.5V~4.35V之间,跟电池电压和充电状态有关。
充电情况下,PMID的输出是输入VBUS减去内部Q1 MOSFET的压降,此时,PMID输出电流能力要看VBUS的输入能力和Q1 MOS导通电阻的承受能力,推荐在3A以内。
还有个问题请教:现在想对外提供5V电源,是对sys进行升压后输出还是直接使用PMID输出?这两个有什么区别?
如果用PMID输出,好处是不需要外部DCDC,充电时VBUS给PMID供电,OTG时电池升压给PMID供电;不好的地方是在充电和OTG切换时PMID会有大概600mS的间隔。
如果用SYS或BAT直接升压,好处是连续不间断;不好的地方是需要增加BOOST DCDC。
在这600ms切换期间,pmid输出电压是不确定的对吗?
如果是这样,那对系统供电的话只能用sys加dc-dc了。