This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

低噪声模拟电路的电源



设计的电路板上需要低噪声的电源,由于系统设计原因,无法使用线性电源。只能是通过直流电源+DCDC模块+LDO来实现,直流电源是CPCI机箱背板提供的12V开关电源,DCDC模块使用金升阳12V转正负15V,3瓦的隔离DCDC模块,LDO使用TI的TPS7A4901DGNT和TPS7A3001DGNT。按照电源厂家的推荐,在DCDC前后都加了1mH的共模电感,电感前后都有10uF的电容。

实际测试的效果,不加LDO,只通过DCDC前后的两个共模滤波电感和电容,可以把DCDC的噪声降到正负10mV以下,过了两个LDO之后,从示波器上来看,没有明显变化。都是用示波器的X1档,交流耦合的方式来看的。想问问是测量的方法有问题,还是说噪声没有办法再降低了?