你好,有个疑问:在boost模式下pmid可以输出5V电压,那么如何在充电模式下能同样对外提供5V电压?我测了在充电状态下pmid只能输出4.4V左右。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,有个疑问:在boost模式下pmid可以输出5V电压,那么如何在充电模式下能同样对外提供5V电压?我测了在充电状态下pmid只能输出4.4V左右。
你用的是哪个料号?
在充电状态下从VBUS到PMID只隔了一个MOS,PMID即可旁路输出,压差取决于MOS RDSON和多大电流。你多大电流压差有5.1V-4.4V=0.7V那么大?
使用的是bq24195.
当时测pmid电压确实是4.4V,这可能和我的输入电压有关系。
但我今天用5v电压输入时,测输入端却是4.9v,隔了一分钟左右又测了一下变成了4.95v,这是为什么?
在充电模式下,PMID没有稳压控制,会跟随VBUS。所以你测到4.9V或4.95V实际上是相当于VBUS减去Q1 MOSFET压降。BQ24195的Q1 MOS的Rds(on)=23mR(typ),大约PMID=VBUS - 23m*I。