电路如上图,我板子上是2个TPS65261-1,其中一个的PGOOD给到另一个,第一个的三个EN管脚都接到输入分压,MODE接V7V输出,上电的时候一个的芯片工作正常,PGOOD正常输出给到第二个芯片,有时候第二个芯片就无输出,也有能输出的时候,无输出的情况下测量三个EN管脚都是大于3V的,V7V也是正常输出6.3V,请问一下这个可能是什么原因呢(虚焊问题可以排除)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电路如上图,我板子上是2个TPS65261-1,其中一个的PGOOD给到另一个,第一个的三个EN管脚都接到输入分压,MODE接V7V输出,上电的时候一个的芯片工作正常,PGOOD正常输出给到第二个芯片,有时候第二个芯片就无输出,也有能输出的时候,无输出的情况下测量三个EN管脚都是大于3V的,V7V也是正常输出6.3V,请问一下这个可能是什么原因呢(虚焊问题可以排除)
你有两个TPS65261-1示意图供我审查吗?当你说第二个芯片没有输出时,哪个轨道没有输出,你能告诉我那个轨道的VIN、EN和LX波形吗?

第一个的原理图,其实两个的原理图是一样的,只是第一个的EN3接的V7V(这边就遇到个问题,我EN3接V7V的时候第一个也不输出,三个电源轨都没输出,万用表测量V7V有6.3V输出,后面我把EN3接到输入分压R183那里才有输出的);第二个芯片也是没输出的时候三个电源轨都没输出,测量V7V输出正常,ENX也是高电平,目前我把输入分压电阻(两个芯片的)改小R182从100k改为43K,暂时都有输出,反复测了几十次目前输出正常,示波器测量输入VIN和V7V的波形发现V7V输出比输入还上升得快,会不会是这个原因导致时序不太对导致的没输出,但是有点没搞明白V7V的输出为啥会比输入上升更快
感谢您的详细反馈。但是为了澄清一下,你能在输出正常的情况下给我分享一下原理图吗?在没有输出的情况下也能给我分享一个原理图吗?
我们不建议将EN与VCC连接:EN需要外部电源来启用设备。在降压开启之前,VCC引脚上没有电压,因此您无法用0V EN开启降压。您可以将电阻分压器与VIN一起使用。